Easy mounting of ball pins by hand, thanks to the clip-on spherical bearing bushing from igus2015-07-13
The new lubrication- and maintenance-free igubal® clip-on spherical bearing bushing (ZCLM 06-10) from igus can be easily mounted manually. The '06' stands for a ball pin of size M6 and the '10' stands for the plate thickness of the holding fixture in millimetres. A cylindrical bore with 12 millimetre diameter, is all that you will need. "The ball pin is inserted into the bushing, then simply pushed until it clicks into the holding fixture," says Thomas Preissner, Product Manager of the igubal spherical bearings division at igus, while explaining the novelty. "Typical application areas for this are coupling rods, double spherical bearings or other solutions for driving connecting rods. The nice thing is that the designers have great freedom in designing their geometries." Inside the bushing there is a spherical holding fixture for the ball pin, that securely holds it in position. igus offers the matching ball pin in galvanised or stainless steel. |