World's first for long travels: 40 percent lighter cables for e-chains2015-07-12
Whether in plant construction, mechanical engineering, cranes, ships or conveyor technology, the travel distances in dynamic applications are becoming increasingly longer whilst speeds and number of movements are rising. This leads to everincreasing stress on cables that are constantly in motion. The motion plastics specialist igus has developed extremely lightweight single core motor cables for energy chains for long travels, the chainflex types CF430.D and CF440. By the use of a special stranded conductor, the cables are up to 40 percent lighter than standard copper cables. Depending on the cable length and cross-section, the savings potential of the new motor cables can be up to several tonnes, offering a considerable saving on required drive force. |