The solution
Originally, the conveyor was supplied with energy and signals on its 366m long track via a motor cable drum. Now a modern energy chain system from igus performs this task. Since the length of the travel results in push/pull forces that should not be underestimated, the project engineers recommended the use of a rol e-chain that does not glide in the guide trough but rolls over high-strength rollers with stainless steel ball bearings. Due to the unfavourable ambient conditions, a
Heavy Duty rol e-chain® type 5050RHD is used. External radius stop-dogs prevent the conveyed material from getting stuck. In addition, the guide trough was equipped with an enclosure as a protection against rising and weather.A floating moving end suspension also ensures lateral tolerance compensation, and an igus Condition Monitoring System ensures the high availability that is indispensable in this application. The system continuously measures the push/pull forces that occur. If obstacles or blockages occur during the movement of the energy chain, they are detected by the i.Sense and the system can then ensure an immediate stop of the conveyor. In this way, major damage, such as tearing off of cables, is avoided.