배송 위치를 선택하세요.

국가/지역 페이지 선택은 가격, 선적 옵션 및 제품 가용성과 같은 다양한 요인에 영향을 줄 수 있습니다.
담당자
한국이구스

인천광역시 연수구 벤처로

12번길 42

+82 32 821 2911
+82 32 821 2913
KR(KO)

Plain bearings for individually adjustable assembly supports in automotive engineering

iglidur plain bearings in car assembly combine load capacity, flexibility and low weight

For the development of an assembly support, which was for use in an assembly line in the automotive industry, the project managers decided on the use of iglidur polymer plain bearings. The plain bearings allow pivoting, rotating and sliding application. They are highly resilient, require little maintenance and allow a long service life. Unlike steel bearings, they combine these advantages with exceptionally low weight, which was explicitly desired in this application.

Profile

  • What was needed: iglidur polymer slewing ring bearings
  • Requirements: Assembly support had to be pivotable, rotatable and slidable, the plain bearings had to be lightweight and at the same time highly loadable as well as requiring little maintenance and guaranteeing a long service life
  • Industry: Automotive industry
  • Success for the customer: Approx. 60 assembly supports were successfully fitted with the polymer plain bearings; they combine the desired weight saving with the high demands on load-bearing capacity, flexibility and service life
Assembly support Assembly support with console

Problem

In assembly lines such as in the automotive industry, assembly supports are used on which the vehicle is gradually assembled in several steps. In such an assembly line, such an assembly support had to be developed for the assembly of centre consoles of passenger cars (Ford). Due to the high degree of flexibility required, high demands were placed above all on the plain bearings in the application. In order to be able to carry out all the necessary assembly activities in the best possible way, the assembly support had to be able to pivot, rotate and slide. Due to the use on an existing assembly line and for ergonomic reasons, a further focus was on keeping the weight of the assembly supports as low as possible. In addition, it and all of its components had to be highly resilient, require little maintenance and still have a long service life.

Solution

Möve-Metall GmbH, which was responsible for the construction of the assembly support, worked with plain bearings from our product portfolio in order to implement the points described in the problem. Specifically, it was decided to use an iglidur polymer slewing ring bearing (PRT-01-100). The function of the bearing is to enable the rotary movement of the assembly support. The decisive advantage of the PRT polymer slewing ring bearing over the steel slewing ring ball bearing otherwise used for this application is in particular its significantly lower weight. Further characteristics are a high load capacity, low necessary maintenance as well as a long service life and high corrosion protection. Today, a total of approx. 60 such assembly supports with the polymer slewing ring bearings are in production use.
PRT-100 view from below View of the assembly support with slewing ring bearing from below
Assembly support 3D
Assembly support 3D


용어 "Apiro", "AutoChain", "CFRIP", "chainflex", "chainge", "chains for cranes", "ConProtect", "cradle-chain", "CTD", "drygear", "drylin", "dryspin", "dry-tech", "dryway", "easy chain", "e-chain", "e-chain systems", "e-ketten", "e-kettensysteme", "e-loop", "energy chain", "energy chain systems", "enjoyneering", "e-skin", "e-spool", "fixflex", "flizz", "i.Cee", "ibow", "igear", "iglidur", "igubal", "igumid", "igus", "igus improves what moves", "igus:bike", "igusGO", "igutex", "iguverse", "iguversum", "kineKIT", "kopla", "manus", "motion plastics", "motion polymers", "motionary", "plastics for longer life", "print2mold", "Rawbot", "RBTX", "readycable", "readychain", "ReBeL", "ReCyycle", "reguse", "robolink", "Rohbot", "savfe", "speedigus", "superwise", "take the dryway", "tribofilament", "triflex", "twisterchain", "when it moves, igus improves", "xirodur", "xiros" 및 "yes" 는 독일 및 일부 외국에서 igus® GmbH/ Cologne의 법적 보호를 받는 상표입니다 이는 독일, 유럽연합, 미국 및/또는 기타 국가 또는 관할권에서 igus GmbH 또는 igus의 계열사가 보유한 상표(예: 출원 중인 상표 또는 등록 상표)의 전체 목록이 아닙니다.

igus® GmbH는 Allen Bradley, B&R, Baumüller, Beckhoff, Lahr, Control Techniques, Danaher Motion, ELAU, FAGOR, FANUC, Festo, Heidenhain, Jetter, Lenze, LinMot, LTi DRiVES, Mitsubishi, NUM, Parker, Bosch Rexroth, SEW, Siemens, Stöber 및 이 웹사이트에서 언급된 다른 모든 드라이브 제조업체의 어떠한 제품도 판매하지 않음을 알려드립니다. 이구스에서 공급하는 제품은 igus® GmbH의 제품입니다.